This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART Ring Indicator signal active low or active high?

Hi,

I have the following question:

Is the "Ring Indicator" Signal from the UART1 ative low or active high?
From the signal naming ("UARTx_RIN") it is not clear because the "N" at the end is not a "n" like on CTS ("UARTx_CTSn") for example.
In table 19-8 the Type is "1". What does this Type mean?
This is based on SPRUH73G.

Thanks and best regards,
Patrick