Other Parts Discussed in Thread: OMAP-L138, ADS901
Hi,
I am using OMAP-L138 EVM and ADS901 which has interfaced with User Interface (UI) board. I have few queries, please help me out.
1. How can I set the sampling rate to 10 kHz for this ADC ?
2. How to run OMAP-L138 evm at 456-MHz ?
3. What is the default clock frequency of uPP ? How can I modify the clock to increase or decrease the speed of uPP ?
I will appreciate your quick response.
Thanks.
Tariq