- OMAP3530/3525 -Future DM based deviceswill provide similar functionality as the OMAP3530 and 3525. Beyond these, there are several high-performance, multimedia-focused devices in the DaVinci platform that are in development that will offer even greater video and media performance. These devices will also use the ARM Cortex-A8 processor so application software compatibility can be preserved.