Hi ,
I am able to build the Debug Build Image for WinEC7(OMAP4430) and I have a crash in kernel after loading the pm.dll.
Log messages which i am getting are:
PID:00400002 TID:00920006 -OEMIoControl(rc = 1)
PID:00400002 TID:00920006 InitializePMExtension: Can't find 'PmExtPath' key.
PID:00400002 TID:00920006 OSAXST1: >>> Loading Module 'ccfgsvc.dll' (0xC040B1F8) at address 0xEEB10000-0xEEB3D000 in Process 'NK.EXE' (0x90611AD0)
PID:00400002 TID:00920006 DEVICE!RegReadActivationValues RegQueryValueEx(Drivers\BuiltIn\MUsbOtg\DllName) returned 2
PID:00400002 TID:00920006 DEVICE!I_ActivateDeviceEx: can't find all required activation values in 'Drivers\BuiltIn\MUsbOtg'
PID:00400002 TID:00920006 DEVICE!RegReadActivationValues RegQueryValueEx(Drivers\BuiltIn\FlashDisk\DllNamPID:00400002 TID:00920006
PID:00400002 TID:00920006
e) returned 2
PID:00400002 TID:00920006 DEVICE!I_ActivateDeviceEx: can't find all required activation values in 'Drivers\BuiltIn\FlashDisk'
PID:00400002 TID:00500002
After this it is going to IdleState and not launching the shell.
Any help is appreciated.