Hi,
My current design makes use of two C6678 DSP with one UCD9222 and one UCD7242 supplying each DSP with its own CVDD voltage rail.
I did a power consumption estimate for the C6678 DSP and found out that the UCD9222 and UCD7242 10A per 1.0V rail power solution for the Evaluation board was at its limit for the default configuration of the "C6678 Power Consumption Summary Rev 2.0" document found in the TI website.
I used the "C6678 Power Consumption Summary Rev 2.0" to estimate the worst case power consumption and current draw for the C6678 DSP. However, the default configuration of the DSP in the excel sheet states that the current draw for CVDD is already 9455.26mA. However the UCD7242 can only supply 10A for each voltage rail. The Evaluation board uses only one rail to supply the 1.0V CVDD output. My board will also do the same with each DSP receiving a maximum of 10A. Hence, according to the excel sheet, the evaluation board is already running close to its limit for the given parameters.
I noticed that the Case Temperature make a huge difference to the Baseline current draw for the CVDD. If I were to run my DSP at the stated 85 degrees C, it will meant that the power solution of the Evaluation Board will be insufficient as it is drawing close to the limit of the UCD7242. If the core utilization is at 50%, the current draw will be over 10A. The only way that it it runs well under 10A is if the case temperature is lowered. This could be the case if the evaluation board is not meant to be run at higher temperatures.
Am I calculating the power consumption correctly?
If so, the evaluation board's power solution appears to be inadequate for intensive processing to be carried out on the board itself. May I find out TI's recommended power solution for intensive computation to be carried out on the C6678?
The hardware design guide gives a reference schematic for one UCD9222 and two UCD7242 with tied outputs. This solution will mean that I will have to use 4 large inductors and that will take up more of space in my design, in which I cannot afford.
The current UCD9222 and UCD2742 power solution recommendation appears to be only suitable lower case temperatures.
Regards,
Allan