Other Parts Discussed in Thread: AM3354
Hello,
is it possible to use the AM3354 ZCE and the ST Micro MT29F NAND Flash with 16-Bit? I have also connected a LCD like the starterkit AM335x (24Bit RGB, LCD_DATAx, GPMC_Ax) .
Can i use 3,3V for the LCD (LCD_DATAx, GPMC_Ax) and 1,8V for the NAND (GPMC_Ax) with the 8-bit NAND?
And last whats a typically size for the files in NAND to boot Android or Linux from the NAND Flash into RAM?
Thanks
Stefan