Hello,
I checked the example code (led blinking and rtc) on c6748 LCDK kit (Burn the code via uart 2 and boot from NAND).
But after some time (not fixed time like 30 secs, 50 seconds, 80 secs etc) code not work , it look like a hang . When I reset the kit via reset button. Then it still in hang condtion.
But when I removed the power (5V DC) and again applied, then it start working but hang again .This process repeated again and again.
For the reference I attached .bin and .out files and .cfg file which loaded for making the .bin file via AISgen tool.
regards
Sachin Arora