Hi,
Iam using M29F2G216ABBEHC-2Gb 16bit Nand Flash.
Can i use Nand flash as 8bit Nand flash i will ignore upper 8bits. As 8bit NAND flashdrivers are available in MCSDK\...NANDWRITER.
In Pdk\....evm66x_Nand.h contains page count=32, block count=4096 page size=512
I needs to change pagecount=64, block count=2048, page size= 1024 in Nand.h
Iam able to change above by commenting ifndef condition but effect is not resulted during debugging.
How to build modified Nand.h ?
regards,
SrinivasaPrasad.