This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CLK Clockspeed Calculations

I am using a timer on the DM6467 to calculate some statistics reporting on multiple platforms. Each platform runs its respective DSP at a different clockspeed (I believe 600Mhz and 729Mhz). I am using the clock manager family of functions to capture the correct clock speed. in particular  CLK_countspms() . I am noticing a drift in my statistics which I think I can attribute to the difference in clock speed. I believe that maybe the values used in the CLK functions could be incorrect for one of the platforms.

A few questions. Is it possible to look at the source of these functions to see what they're doing thus providing me a little more info? I believe I am running with BIOS version 5. Also, If I could find out how and where this clock speed value is defined I could simply change that for the correct platform. I have seen some mentioning in the .tcf file associated with the project, but I am unfamiliar with the fields used. Alternatively, is there another method I could use for clock speed calculations?

Thanks,
Mark