Other Parts Discussed in Thread: TMS320C6678
This is a general question pertaining to the differences in the accessable onboard emulation for TI-EVMs
For example lets consider TMDSEVM6678LE - TMS320C6678 Lite Evaluation Module with XDS560V2 Emulation and TMDSEVM6678L - TMS320C6678 Lite Evaluation Module which has a $200 price difference. I would assume by purchasing the EVM with XDS560V2 this would allow me to use a USB cable connected to the EVM and then to my computer running CCSv5 and get the faster more flexible XDS560v2 emulation for debugging/inspection? is this correct? I am confused because when I look at the external sites product images I see things like:
http://www.einfochips.com/images/tmdxevm6657le.png which leads me to believe this assumption but the confusion comes from sites like this http://www.advantech.com/Support/TI-EVM/6678le_of.aspx which do not show this extra daughter card attached in the product photo.
I think I am missing something here and would like to be enlightened on this topic. Also I recall speaking with a TI engineer awhile back that said the free license with CCS only allows connection to the board via XDS100. I am a student doing a research project under my professor and am using CCSv5 under the free license. If this is true then it would not seem necessary to buy the EVM with XDS560v2, but no where on the product info is this little bit of licensing detail mentioned...