This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Max div value check for DM814x MDIO Control Register bug?

Hi,

The DM814x TRM, sec. 9.4.2.2 says that the CLKDIV parameter in the "MDIO Control (CONTROL) Register" is bits 15 downto 0.  But the check in drivers/net/davinci_mdio.c is against 0xFF:

#define CONTROL_MAX_DIV (0xff)

....

static void __davinci_mdio_reset(struct davinci_mdio_data *data)
{
         u32 mdio_in, div, mdio_out_khz, access_time;
         mdio_in = clk_get_rate(data->clk);
         div = (mdio_in / data->pdata.bus_freq) - 1;
         if (div > CONTROL_MAX_DIV)
                 div = CONTROL_MAX_DIV;


Is it a coding bug, or should the divider really stay at 0xFF and below?
Dan -