Hello,
I am trying to import CSL v2.5 examples from CCS v4.2.4 to CCS v5.3 without success (I have the ezc5535 board).
It seems that the path for CSL are not defined the same way on CCS5.3 and on CCS v4.2.4
In CCS v4.2.4, path are defined in properties / C-C++ builder / Macros
In CCS v5.3 I dont not have find the path for the linker, so I have errors when trying to call CSL 2.5 API function.
Does any one can help me ?
Thanks.
Nicolas