This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UPP Control Pin Usage

Hello,

The pins  (Clk, Start, Enable and  Wait) concerning  UPP  timing and control on that C6657 are labeled as either “Channel 0 ” .. i.e.,   UPP_CH0_CLK or “Channel 1 ” .. i.e.,  UPP_CH1_CLK in the C6655/7  data sheet. 

How are these pins associated to the “Channel A” or “Channel B”   designations used extensively in the  UPP User Guide   SPRUHG9 ?  There does not seem to be register for programming  this and  I did not want to simply assume  that “Channel 0” =  “Channel A” and  “Channel 1” = “Channel B.    

It is clear from  SPRUHG9  how DATA and DATAX pins are utilized so there are no questions pertaining to the data lines.

Thank you.