This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Send out packets with NDK



Hey...

I recently worked with the HelloWorld and Client demo and got it to work. Receiving and echoing back packets over ethernet works well! Now I want to send packets to my host PC anywhere in my project code, and not only  in the deamon call back, where incoming packets are received from the PC. For this, I create a socket, and send out the packets: I see traffic on my ethernet switch, but the packets do not appear in my wireshark session!!!

What am I doing wrong??

     SOCKET  s;
     struct  sockaddr_in sin1;
     struct  sockaddr_in sin2;
     int     i,tmp,test;
     char    *pBuf = "Haba dere!";
     UINT32  buffersize = 11;
     struct  timeval timeout;
     HANDLE             hBuffer;

     /* Allocate the file environment for this task */
     fdOpenSession( TaskSelf() );

     // Create test socket
     s = socket(AF_INET, SOCK_DGRAM, IPPROTO_UDP);
     if( s == INVALID_SOCKET ) {
          printf("failed socket create (%d)\n",fdError());
          goto leave;
     }

     // Bind socket
     bzero( &sin1, sizeof(struct sockaddr_in) );
     if( bind( s, (PSA) &sin1, sizeof(sin1) ) < 0 ) {
         printf("failed bind (%d)\n",fdError());
         goto leave;
     }

     // Prepare address for the SendTo
     bzero( &sin1, sizeof(struct sockaddr_in) );
     sin1.sin_family      = AF_INET;
     sin1.sin_len         = sizeof( sin1 );
     sin1.sin_addr.s_addr = inet_addr(IPAddr);
     sin1.sin_port        = htons(7);


     // Configure our timeout to be 5 seconds
     timeout.tv_sec  = 5;
     timeout.tv_usec = 0;

     setsockopt( s, SOL_SOCKET, SO_SNDTIMEO, &timeout, sizeof( timeout ) );
     setsockopt( s, SOL_SOCKET, SO_RCVTIMEO, &timeout, sizeof( timeout ) );


     while(1) {
             if( sendto( mysocket, mypBuf, buffersize, 0,(PSA)&mysin1, sizeof(mysin1) ) < 0 ) {
                printf("send failed (%d)\n",fdError());
                break;
             }
             else {
                printf("send successful  !\n");
             }
      }