This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 EVM gel file DMtimer regsiter base addresses

Genius 9355 points

I'm investigating an issue with dmtimer setting on DM8148 EVM and as a result looked through the DM8148 gel file. The gel file I have shows the following:

#define DMTIMER0_BASE_ADDR     0x4802C000  

#define DMTIMER1_BASE_ADDR     0x4802E000  

#define DMTIMER2_BASE_ADDR     0x48040000  

#define DMTIMER3_BASE_ADDR     0x48042000  

#define DMTIMER4_BASE_ADDR     0x48044000  

#define DMTIMER5_BASE_ADDR     0x48046000  

#define DMTIMER6_BASE_ADDR     0x48048000

 #define DMTIMER7_BASE_ADDR     0x4804A000

 

However, the DM8148 datasheet on the web (Sept 2012) version shows the following in table 2-6:

0x4802_C000 0x4802_DFFF 0x0802_C000 0x0802_DFFF 8KB Reserved

0x4802_E000 0x4802_EFFF 0x0802_E000 0x0802_EFFF 4KB TIMER1 Peripheral Registers

0x4802_F000 0x4802_FFFF 0x0802_F000 0x0802_FFFF 4KB TIMER1 Support Registers

 

The gel file numbers the timers as 0-7 whereas the datasheet uses 1-8 however timer0 address of 0x4802C000 is reserved so this is not going to work.

 

Rgds

-Dipa-

 

  • Hi Dipa,

    The Gel file does not use any of DMTIMERx_BASE_ADDR defined so it must be an overlook when Mistral porting the Gel file from other project.  We will fix the Gel file by removing them.  . 

    In the future, the DS should always cheat as a superset over TRM and SW.

    BR,

    Viet