Other Parts Discussed in Thread: TMS320DM6467T
Hi,
I am working with TMS320DM6467T and there is guide which has the steps on "Davinci Installation". As given, I have downloaded the 'flash_utils.tar.gz' for UBL.
In one the steps, its mentioned to select the 'ublDavinci.pjt' file and build the UBL '.out' file. I am using Eclipse based CCS 5.11 and I have migrated the given project in 5.11 Version, but it shows the following errors.
How do I resolve these errors?
And, after removing these errors and building the UBL ELF (.out file) , do I have to follow the same procedure given in the guide for generating binary file(.bin) or are there utilities in CCS 5V+ for generating (.bin) file?