This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Android JB 4.2 wl12xx

Hello.

Kernel: 2.6.32 (FROM SEMC Sony....)

Wifi/BT/FM: in JB4.1 used wl12xx.ko and wl12xx_sdio.ko and works everything.

History:

As You know in JB4.2 bluez was removed ad Google add Bro..com Bluedroid stack.

Wifi working perfectly with above module and wl1271-fw-multirole-roc.bin firmware. For bluetooth i use binary firmware from ICS TIInit_7.6.15.bts and TIInit_7.5.20.bts

Strange is that i can turn on bluetooth and turn off but when i try to scan other device i do not see nothing the same is when i try to scan from other device my device.

I have only problem with bluetooth and FM. As FM i do not use as bluetooth i need. 

Is someone can help me with this problem?