Hi
I have connected HDMI Audio Out to MCBSP 2 where MCBSP is the slave as the other Device is giving Clock to Omap
When I Record and play the wav file it is always empy.
Below are mcbsp Dump Register values
953.798736] **** McBSP2 regs ****
[ 953.802246] DRR2: 0x927dfb38
[ 953.805419] DRR1: 0x0000
[ 953.808197] DXR2: 0x0000
[ 953.810974] DXR1: 0x0000
[ 953.813781] SPCR2: 0x0230
[ 953.816558] SPCR1: 0x0031
[ 953.819335] RCR2: 0x8041
[ 953.822143] RCR1: 0x0040
[ 953.824920] XCR2: 0x8041
[ 953.827697] XCR1: 0x0040
[ 953.830474] SRGR2: 0x001f
[ 953.833282] SRGR1: 0x0f00
[ 953.836059] PCR0: 0x000f
Is there any configuration I am missing?
Thanks
Kavitha