Linux-2.6.32.17-davinci1 uImage is not displaying mtd nand partitions ...what can be the reason...what and where i n the kernel i need to do modification to see the partitions for bootlader, kernel and filesystem...
please suggest
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Linux-2.6.32.17-davinci1 uImage is not displaying mtd nand partitions ...what can be the reason...what and where i n the kernel i need to do modification to see the partitions for bootlader, kernel and filesystem...
please suggest
Thomas,
I use Spectrum Digital dm368 board. I cant show logs, cuz this time all working fine. I closed EM_SEL pin with vcc3.3 for EMIF testing and forgot about this. Then I tried to flash bootloaders, u-boot, kernel and fs. I had no problems with bl's, u-boot and kernel. I had problems only with fs, cuz kernel didnt detect any mtd blocks. I used cat /proc/mtd . After, I unlocked EM_SEL and kernel detect mtd blocks without any problems.