This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C64x+ atomic operations on C6474?



Does the C6474 support the atomic operation primitives that are described in SPRU732J section 9 (LL-SL-CMTL)?

If so, are there constraints on the address(es) that are used with these instructions, or any constraints on other nearby instructions (beyond the rules mentioned in SPRU732 about only the .D2 unit being able to execute synchronization primitives, only one being allowed per execution packet, and the sequencing of the synchronization primitives)?

The source code from the IPC RTSC package (ipc_1_24_03_32/packages/ti/sdo/ipc/gates/GateAAMonitor_asm.s64P) mentions some megamodule errata, but I can't find the "GEM DATA MEMORY CONTROLLER" document it mentions, so I'm not sure if they apply to the C6474.

  • No, that's only supported in the shared memory of the C6472 and TCI6486.  Please note that Atomic instructions tend to be used for Semaphore type operations, and the C6474 has a Hardware Semaphore block as opposed to implementing the LL/SL/CMTL.

    Best Regards,

    Chad