This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm3xx_sd_boot-6.1 and DM368



Hello,

I am using the SD card flashing tool v. 6.1 on a custom board with a DM368.  Whenever I try to boot from an SD card, if there is a bad block in NAND in the area that the kernel gets written to, everything fails because the kernel doesn't get completely written.  I see no code in sdcard_flash .c to skip bad blocks, even though they are marked during the erase.  Also, in sdboot_flash_cfg.h I see the following code:

#define KERNEL_FLASH 0x400000
#define ROOTFS_FLASH 0x600000

and

#define KERNEL_SIZE (3*MB)
#define ROOTFS_SIZE (4*MB)

So it seems like the ROOTFS will be stepping on the KERNEL.  Am I missing something?