I have a custom board based on AM3352.
But not boot by using uart0 that is't print "CC" and download boot's img with jtag , then it configure sysboot at NAND boot
But don't yet.
Now it is verify sysboot configuration (uartboot or nandboot ) with jtag 's control_register memory map
and
Forums search same problem ( http://e2e.ti.com/support/dsp/sitara_arm174_microprocessors/f/791/t/237315.aspx) and any problem
it 's checks
we doubt that EVM is when high then sysboot swtich at 3.1V but custom board is when high then sysboot swtich at 2.3V.
and VDDS Voltage is 3.3 V but EVM is 1.8V.
and Voltage sequence is different with EVM and Custom board
Custom board isn't using POWER MANAGEMENT IC
it 's wrong .
Thank you
Kind Regards,