Hi,
Running DM8148EVM with EZSDK 5.05.01.04.
I am trying to run the saLoopback sample app but it's failing with the following error:
Driver Name: ti81xxvin
Driver bus info: TI81xx Platform
DriverVPSS_DCTRL: venc 1 already stop
is capable of doing capture
saLoopBack:
Mode set is 0
Setting DV Preset failed
I have followed the instructions in the Software Developers Guide and the instructions for running the samples in the PSP Video Capture Driver User Guide at http://processors.wiki.ti.com/index.php/TI81XX_Video_Capture_Driver_User_Guide but I still cant get the sample to work.
I have a 1080i camera connected to the component input on the EIO board. This works ok and I can see captured video on the LCD display if I use the OMX capture_encode_a8host_debug.xv5T example app. But I cant get the V4L samples to work.
Thanks,
Steven