hello, everyone.
During the situation when my program CODE had loaded into external SDRAM and the CODE execute from external SDRAM, I need to reconfigure C674x PLL to lower the PLL out from 600M to 400M, can I keep SDRAM context same as before. I know the SDRAM have a refresh time, such as 64ms, During the PLL reconfiguration, the SDRAM refresh can continue?if it can not continue, the SDRAM context will lost no doubt, which worry me very much.
someone help!