Other Parts Discussed in Thread: AM3505
Hi
We have a custom design of AM3505 on linux kernel 2.6.32.
Now we are migrating to linux kernel 2.6.37. I am able to generate uImage for this new kernel + old driver file.
But while booting with is uImage I am getting following error.
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option; here are the available partitions:
1f00 512 mtdblock0 (driver?)
1f01 1792 mtdblock1 (driver?)
1f02 256 mtdblock2 (driver?)
1f03 5120 mtdblock3 (driver?)
1f04 1040896 mtdblock4 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
[<c008000c>] (unwind_backtrace+0x0/0xec) from [<c037df14>] (panic+0x54/0x170)
[<c037df14>] (panic+0x54/0x170) from [<c0009140>] (mount_block_root+0x1d0/0x210)
[<c0009140>] (mount_block_root+0x1d0/0x210) from [<c0009220>] (mount_root+0xa0/0xbc)
[<c0009220>] (mount_root+0xa0/0xbc) from [<c00093a0>] (prepare_namespace+0x164/0x1bc)
[<c00093a0>] (prepare_namespace+0x164/0x1bc) from [<c0008708>] (kernel_init+0x10c/0x14c)
[<c0008708>] (kernel_init+0x10c/0x14c) from [<c007ba78>] (kernel_thread_exit+0x0/0x8)
Can you please help me on this.