Hello, this is a problem experienced during Linux boot but more of a low-level/hardware issue so hopefully this is the right forum.
I have an intermittent hang during boot on DM365, traced to the first access of AEMIF registers in davinci_nand.c, which is a read of A1CR during probe. JTAG debug (OpenOCD) is unable to halt the CPU while in this state. This only seems to happen when powered on from cold, if the reset line is toggled when already powered up then it's OK.
This is on our latest PCB revision, the previous one seemed OK.
Bit of a long shot asking here but thought I would in case it rang a bell with anyone - maybe we just have some power supply sequencing or reflow problems or something to find.