All,
I used MVL 2.6.18 kernel on dm365
In Power on/off test, sometimes the following error message is occured
and kernel hanging.
What kind of problem in kernel ?
=============================================================
TVP5150 channel0 Video Decoder I2C driver 0-005d: tvp5150am1 detected.
TVP5150 channel0 Video Decoder I2C driver 0-005d: Rom ver is 4.0
BUG: unbalanced irq-handler preempt count in i2c_davinci_isr+0x0/0x220!
Bad mode in interrupt handler detected: mode UND_32
Internal error: Oops - bad mode: 0 [#1]
Modules linked in: davinci_gpio dm365mmap edmak irqk cmemk
CPU: 0
PC is at vprintk+0x26c/0x420
LR is at 0xc0577c0c
pc : [<c004f87c>] lr : [<c0577c0c>] Tainted: P
sp : c3145fe0 ip : a000009b fp : c3145ea4
r10: 0000004b r9 : c3144000 r8 : 00000001
r7 : 00000001 r6 : c03ab8ef r5 : c3145ec4 r4 : 00000000
r3 : 6000001b r2 : 00000000 r1 : 6000001b r0 : c0340ba8
Flags: nZCv IRQs on FIQs on Mode UND_32 Segment user
Control: 5317F
Table: 83140000 DAC: 00000015