I have following questions about the ARM (AM3359) internal access time by L3 and L4.
I would be very happy, if someone could answer.
Which interface should be applied for an interconnection between ARM and memory-units?
L3 or L4? Are the L3 and L4 applications configurable?
How long does ARM (Cortex-A8) access-time take to write/or read a Byte (or Double word) on 64K Shared Memory?
How long does ARM (Cortex-A8) access-time take to write/or read a Byte (or Double word) on 64K RAM Memory?
How long does ARM (Cortex-A8) access-time take to write/or read a Byte (or Double word) on PRU 12K Shared Memory?
How long does ARM (Cortex-A8) access-time take to write/or read a Byte (or Double word) on PRU0/1 8K Memory?
Is the ARM has the same access time for all these memory-units!?
Best regards
Rouzbeh