This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCASP0 Revision Register not consistent with TRM.



Hi,

I am debugging / bringing up MCASP0 on the DM8148 and noted that the  Revision Identification Register (REV), Figure 16-37 of the TRM.  The register appears to be reading back as 0x44307302 while the TRM says it should be 0x44300A02.  Is this an issue?

-Mike

  • Hi Mike,

    This is not an issue.

    The MCASP0 PID register is giving the McASP module revision number that is integrated into the DM814x device. I have a DM8148 2.1 device, and I also read back 0x44307302 from this register (at address 0x48038000).

    I think the TRM is giving the McASP module revision number for DM814x 1.0 device (0x44300A02).

    Best Regards,

    Pavel

  • Hi Mike,

    Thanks for letting us know.  We will fix the TRM in next release.  This error should not cause any issue.

    BR,

    Viet