Other Parts Discussed in Thread: AM3703, TPS65951
We got this issue with approx. 15% of our new manufactured boards, which are unprogrammed. What we already know:
Supply voltages present: VDD1 & VDD2 = 1V2, VIO = 1V8, VRTC.OUT = 1V5. VBAT is ~ 3V8
26 MHz Clock present at PMU 2-3 ms after startup, 32.768 kHz RTC-Clock present at PMU
CLKREQ from AM3703 to PMU is HIGH (not active)
PMU (TPS65951) NRESWARM & NRESPWRON are HIGH (not in reset)
That means power sequencing as in datasheet chapter 6.5.4.2 is complete & fine
We have no external RTC, no USB present, no charger present,
Boot Mode is set to Master (Boot1 with 10k pull-down o GND, Boot0 with 10k pull-up to VBAT (3V8))
Here is a part of the schematic:
I would like to know why INT1 at some of our boards is permanent low, after power up. The system does not boot
The only output at Uart3 is
U-Boot SPL 2012.07 (Oct 25 2012 - 10:13:30)
Texas Instruments Revision detection unimplemented
Than nothing happens, INT1 keeps low.
This indicates the processor has no software, but the software is present on a SD card (working on other boards)
Thanks for any hint
Thomas