This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The requirement of external clock source on AM335x

Guru 10570 points
Other Parts Discussed in Thread: AM3352, OMAP3530

Hello.

I would like to use external clock source for OSC0 XTALIN on AM3352.
Although I can find the crystal requirement on the datasheet(sprs717d P100),
I can not find the requirement of external clock source.

I would like to clarify about following:
  - Absolute maximum ratings of XTALIN pin [V MIN & MAX]
  - High-level input voltage(Vih) [V MIN]
  - Low-level input voltage(Vil) [V MAX]
  - Allowable transient overshoot voltage[V MAX] and time[nsec MAX]
  - Allowable transient undershoot voltage[V MIN] and time[nsec MAX]
  - Period jitter[nsec MAX] or allowable error rate[ppm MIN & MAX]
  - Typical load capacitance value [pF Typ]
  - Pulse width high time and low time [nsec MIN]
  - Transition time [nsec MAX]

Could you provide me these informations?

Best regards,
RY