This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Android does not come up after increasing memory for ducati in kernel



Hello All,

I am working on a custom board based on OMAP4460. The Android release used is 4AI-1.4.

We want to increase the memory allocated for ducati by 10MB.

In the kernel we made the following change, in the file arch/arm/mach-omap2/omap4_ion.h

#define PHYS_ADDR_DUCATI_SIZE   (SZ_1M * 105) to (SZ_1M * 115).

But after making the change we are observing the following crash

[   11.196807] omap-rproc omap-rproc.1: Loaded BIOS image ducati-m3.bin, size 5572820
[   11.206054] omap-rproc omap-rproc.1: BIOS image version is 2
[   11.248413] omap_hwmod: ipu: failed to hardreset
[   11.253631] omap-iommu omap-iommu.0: ducati: version 2.1
[   11.266448] omap-rproc omap-rproc.1: remote processor ipu is now up
[   11.282104] omap_rpmsg_mbox_callback: received echo reply from ipu !
[   11.288848] omap-rproc omap-rproc.1: rproc_mmu_fault_isr
[   11.294708] omap-iommu omap-iommu.0: ducati: errs:0x00000002 da:0x1a800008 pgd:0xe896c6a0 *pgd:px00000000
[   11.305053] omap_rpmsg_mbox_callback: received echo reply from ipu !
[   11.311859] omap_rpmsg_mbox_callback: received echo reply from ipu !
[   11.318664] omap_rpmsg_mbox_callback: received echo reply from ipu !
[   11.325439] omap_rpmsg_mbox_callback: ipu has just crashed !
[   11.331542] dump_ipu_registers: REGISTER DUMP FOR REMOTEPROC ipu
[   11.337951] dump_ipu_registers: PC is at f7bff9e4
[   11.343017] dump_ipu_registers: LR is at bbdfd1be
[   11.348022] dump_ipu_registers: pc : [<f7bff9e4>]    lr : [<bbdfd1be>]    psr: fffdd3cf
[   11.348022] sp : f7bedbf8  ip : dff9fdbf  fp : 7b7f5ebf
[   11.362335] dump_ipu_registers: r10: db9fdf9d  r9 : ffffdfff  r8 : f3ffff8f
[   11.370239] dump_ipu_registers: r7 : bbfffd69  r6 : 7dfd9f5f  r5 : f7d8ffaf  r4 : 9fffbfdd
[   11.379516] dump_ipu_registers: r3 : ffffff9f  r2 : fbddf97d  r1 : bfffffd3  r0 : efbeebff
[   11.388366] dump_ipu_registers: Flags: NZCV  IRQs off  FIQs off
[   11.395019] _event_notify: remoteproc: ipu has crashed
[   11.400512] rpmsg_rproc_error: Fatal error in ipu
[   11.406127] rpmsg_rproc_error: Fatal error in ipu
[   11.411132] omap_rpmsg_mbox_callback: ipu has just crashed !
[   11.417388] rpmsg_reset_work: reseting virtio device 0
[   11.423126] rpmsg_resmgr rpmsg0: Enter rprm_remove
[   11.429412] rpmsg_reset_work: reseting virtio device 1
[   11.435119] rpmsg_resmgr rpmsg2: Enter rprm_remove
[   11.440368] rproc_reset_poolmem: invalid pool
[   11.447235] omap-rproc omap-rproc.1: stopped remote processor ipu
[   11.454315] omap-rproc omap-rproc.1: powering up ipu
[   11.460205] virtio_rpmsg_bus virtio2: rpmsg backend virtproc probed successfully
[   11.469207] virtio_rpmsg_bus virtio3: rpmsg backend virtproc probed successfully
[   11.479309] init: cannot find '/system/bin/setup_fs', disabling 'setup_fs'
Is there any other change required in the kernel to increase memory allocated for ducati ?
Thank you for your time.
Any pointers will be helpful.
Thanks and Regards,
Sanjay