Dear Justin,
I gone through the C6670 SRIO User guide and Example program " MulticoreLoopbackExample Project" .
I have read in the user guide that we can control how Hardware segments the packet . (i.e) 8 Bytes to 256 Bytes. I hope it means that SRIO driver is capable segment the packet that that will be sent out.
However I do not find any information in the example code or user guide about this segmentation information fields. Instead I saw the SRIO_MAX_MTU which was set as 256 Bytes in ex program. This information was passed in CPPI Rx config , CPPI Tx config.
Can you please tell us where to pass segment info in order to make driver to do the packet segmentation ?
Thanks & Regards
Rajkumar