This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR3 MEMORY ISSUE

Other Parts Discussed in Thread: TMS320C6678

HI,

     When i am executing the GEL file in the TMS320C6678. The bellow ERROR is show can any one tell why this error is shown. This Error is shown bellow

 C66xx_8: GEL Output: Main PLL (PLL1) Setup ... 

C66xx_8: GEL Output: Error while waiting for GOSTAT bit returning to 0 ...

  • Avinash,

    Why is the title of this thread "DDR3 MEMORY ISSUE"? You have not asked anything about the DDR3.

    This error message means the PLL1 is not being configured. You can view the GEL file that is running by going to the Debug perspective, selecting a device in the Debug window, and then clicking Tools->GEL Files. In the Control Panel window that opens, you can click on GEL Files on the left and see all of the GEL files that are open for the device that was selected. Double-click on the GEL file name to open it in an editor, then you can search for the error message that you received.

    If you want to confirm the speed that your DSP is running, please go to the TI Wiki Pages and search for "DSP clock speed" (no quotes) to find a short article and a project that you can load/run on one core to determine the clock speed that has been set.

    Is this the same board that has the DDR3 problem in this thread?

    Regards,
    RandyP