This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 USB OTG : Issue in host mode



I have configured dm368 for USB OTG mode .

fgrep USB .config  | grep -v '^#'

CONFIG_USB_HID=y

CONFIG_USB_SUPPORT=y

CONFIG_USB_ARCH_HAS_HCD=y

CONFIG_USB=y

CONFIG_USB_DEBUG=y

CONFIG_USB_ANNOUNCE_NEW_DEVICES=y

CONFIG_USB_DEVICEFS=y

CONFIG_USB_DEVICE_CLASS=y

CONFIG_USB_SUSPEND=y

CONFIG_USB_OTG=y

CONFIG_USB_OTG_WHITELIST=y

CONFIG_USB_WUSB=y

CONFIG_USB_C67X00_HCD=y

CONFIG_USB_OXU210HP_HCD=y

CONFIG_USB_SL811_HCD=y

CONFIG_USB_R8A66597_HCD=y

CONFIG_USB_HWA_HCD=y

CONFIG_USB_MUSB_HDRC=y

CONFIG_USB_MUSB_SOC=y

CONFIG_USB_MUSB_OTG=y

CONFIG_MUSB_SCHEDULE_INTR_EP=y

CONFIG_USB_GADGET_MUSB_HDRC=y

CONFIG_USB_MUSB_HDRC_HCD=y

CONFIG_USB_TI_CPPI_DMA=y

CONFIG_USB_MUSB_DEBUG=y

CONFIG_USB_ACM=y

CONFIG_USB_STORAGE=y

CONFIG_USB_STORAGE_DEBUG=y

CONFIG_USB_MDC800=y

CONFIG_USB_MICROTEK=y

CONFIG_USB_SERIAL=y

CONFIG_USB_TEST=y

CONFIG_USB_GADGET=y

CONFIG_USB_GADGET_DEBUG=y

CONFIG_USB_GADGET_DEBUG_FILES=y

CONFIG_USB_GADGET_DEBUG_FS=y

CONFIG_USB_GADGET_VBUS_DRAW=20

CONFIG_USB_GADGET_SELECTED=y

CONFIG_USB_GADGET_DUALSPEED=y

CONFIG_USB_ZERO=m

CONFIG_USB_ETH=m

CONFIG_USB_GADGETFS=m

CONFIG_USB_FILE_STORAGE=m

CONFIG_USB_FILE_STORAGE_TEST=y

CONFIG_USB_G_SERIAL=m

CONFIG_USB_MIDI_GADGET=m

CONFIG_USB_G_PRINTER=m

CONFIG_USB_CDC_COMPOSITE=m

CONFIG_USB_OTG_UTILS=y

CONFIG_NOP_USB_XCEIV=y


After booting, It is initially in the peripheral mode.

cat /proc/driver/musb_hdrc

Status: MHDRC, Mode=Peripheral (Power=20, DevCtl=80)

OTG state: b_idle; inactive

Options: cppi-dma, otg (peripheral+host), debug=0 [eps=5]

Peripheral address: 01

Root port status: 00000000

DaVinci: ctrl=00 stat=0 phy=21d0

rndis=00000 auto=0000 intsrc=00000000 intmsk=00000000

CPPI: txcr=1 txsrc=0 txena=f; rxcr=1 rxsrc=0 rxena=f

Gadget driver: (none)

ep0 (hw0): 1buf, csr 0000 maxp 0000

(queue empty)

I did modprobe g_file_storage and echo F > /proc/driver/musb_hdrc,  to change it to Host mode.

cat /proc/driver/musb_hdrc

Status: MHDRC, Mode=Host (Power=f0, DevCtl=5d)

OTG state: a_host; active

Options: cppi-dma, otg (peripheral+host), debug=0 [eps=5]

Peripheral address: 01

Root port status: 00000501

DaVinci: ctrl=00 stat=1 phy=21f0

rndis=00000 auto=0000 intsrc=00000000 intmsk=01ff1e1f

CPPI: txcr=1 txsrc=0 txena=f; rxcr=1 rxsrc=0 rxena=f

Gadget driver: (none)

But i am getting the below error when i insert a pendrive to usb port ,

musb_bus_suspend 2406: trying to suspend as a_host while active

usb 2-1: new high speed USB device using musb_hdrc and address 10

usb 2-1: device v0421 p0220 is not supported

hub 2-0:1.0: unable to enumerate USB device on port 1

When i reinsert it, i also got an error,

davinci_interrupt 370: VBUS error workaround (delay coming)

From Devctl =5D, it is clear that it is operating in host mode and device is also detected.

I followed procedures mentioned in the link,

https://www.ridgerun.com/developer/wiki/index.php/How_to_configure_DM365_for_USB_host,_device_and_OTG_support

I have enabled the power management in kernel and haved removed J26 jumper.

I am using g_file_storage.ko as i dint find g_cdc_ms.ko mentioned in the link.

i checked the vbus GPIO status using , cat /sys/kernel/debug/gpio , which says  gpio-33  (usb                 ) out hi

If i configure usb as host alone, then the pendrive is mounted.

Please let me know where i am going wrong. 

Is there any other configuration , which i have left out?