This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FFTC Interrupt register

Hi,

we generate an end of packet interrupt on the fftc input queue 0. The interrupt is working, but we cannot determine the source of it because FFTC_ERROR_INTERRUPT_STATUS_REGISTER remains cleared.

This only happens while running on the simulator. When run on hardware the expected bit is set on the above mentioned register.

Is there a problem with the c6670 simulator?

Kind regards

Ralf