Hi,
From the forum posts, some said that "The OMAPL138 contains an ARM9 with a C674x DSP on it." per link:
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/237756/841796.aspx#841796
I see the following kit/evm board at eStore:
1. Texas Instruments OMAP-L138 SOM-M1
OMAP-L138/C6748 DSP Experimenter Kit packaged for Universities (TMDSEXPL138-UNV)
2. Includes two SOMs
- OMAP-L138 SOM-M1 (128 MB mDDR)
- TMS320C6748 SOM-M1 (128 MB mDDR)
OMAP-L138/TMS320C6748 EVM
Item 2 is an advanced version. Why does it have two SOM if L138 has a C674x DSP?
Thanks,