This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

av_server.out problems on DM368 boards

Hi, actually I'm not familiar to TI boards and I'm neither a software engineer, However I have to control this board a little.

I used to change the video&audio configurations with web-based method, such as php.. but now I want to change it with just a simple line of linux command.

the original codes when I can see after applying changes on web is like below (just a part of it)

------------------------------------------------------------------------------------------------------------------------------------------------------

Change in Config Data: Restart AVSERVER!!
killall: Appro_avi_save: no process killed
ApproDrvExit: 7
AVSERVER UI: Stoping.....
isp_get_awb_rgain
isp_get_awb_bgain
Msg_ThrFxn closing...
Kill queue id:131076
AVSERVER UI: Exiting.....
AVSERVER UI: Closed Successfully

CPU CurrentStatus is = 1

*****************************************************************

  IPNC BUILD VERSION: C02_S0103_3.1.4-1

*****************************************************************

./av_server.out DM368 NTSC APPRO2A AEWB 1080P H264 8000000 VBR AUTO MENUOFF P1 2 HQ 1 &
ApproDrvInit: 7
Creat queue id:229380
queue id:229380

AVSERVER UI: Initializing.

 CLK Hz,
 ARM   Hz =  432000000
 DDR   Hz =  340000000
 VPSS  Hz =  340000000
 IMCOP Hz =  340000000

------------------------------------------------------------------------------------------------------------------------------------------------------

I just would like to get this same code using teraterm and linux commands, just like this

# cd /opt/ipnc
# killall appro_avi_save
killall: appro_avi_save: no process killed
# ./av_server.out DM368 NTSC APPRO2A AEWB 1080P H264 8000000 VBR AUTO MENUOFF P1 2 HQ 1 &
#
AVSERVER UI: Initializing.

 CLK Hz,
 ARM   Hz =  432000000
 DDR   Hz =  340000000
 VPSS  Hz =  340000000
 IMCOP Hz =  340000000

>>> DRV_imgsOpen - model file open error !!
>>> default sensor: 1
 DRV LDC: GetConfig 0003 0x0
 [OSA_FILE ] Reading file [/mnt/nand/IMG_Paramset.bin] ... ERROR
IMAGE TUNE: Paramset File is not available..... Setting DEFAULT parameter
 ERROR  (imageTuneCommunication.c|IMAGE_TUNE_ServerOpen|119): IMAGE TUNE 2
 ERROR  (drv_imageTune.c|DRV_imageTuneInit|86): IMAGE_TUNE_ServerOpen()
 ERROR  (drv.c|DRV_init|77): IMAGE TUNE init
 ERROR  (drv.c|DRV_init|111): DRV_init()
 ERROR  (avServerApi.c|AVSERVER_init|574): DRV_init()
 ERROR  (avServerUi.c|UI_start|58): AVSERVER_init()

and it stopped. I just found that differences may occur from the beginning or the code, such as

ApproDrvExit: 7
AVSERVER UI: Stoping.....
isp_get_awb_rgain
isp_get_awb_bgain
Msg_ThrFxn closing...
Kill queue id:131076
AVSERVER UI: Exiting.....
AVSERVER UI: Closed Successfully

CPU CurrentStatus is = 1

and I searched for setting these command but found nothing, so I'm writing on this forum

can someone terminate my stupid process? :(