This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB does not work in U-Boot for AM335xEVM board

Hi there,

I try to enable USB support in U-Boot for the AM335x eval board.

Therefore I modified am335x_evm.h to this:

#define CONFIG_USB_MUSB_AM335X 1

#define CONFIG_MUSB_HCD 1

/* #define CONFIG_MUSB_UDC 1 */

#ifdef CONFIG_USB_MUSB_AM335X

#ifdef CONFIG_MUSB_HCD
#define CONFIG_CMD_USB

#define CONFIG_USB_STORAGE
#define CONGIG_CMD_STORAGE

#define CONFIG_CMD_FAT

#ifdef CONFIG_USB_KEYBOARD
#define CONFIG_SYS_USB_EVENT_POLL
#define CONFIG_PREBOOT "usb start"
#endif /* CONFIG_USB_KEYBOARD */

#endif /* CONFIG_MUSB_HCD */

Then I rebuilt U-Boot but USB still does not work after starting it with "usb start".

This is what I get from usb reset and usb info:

U-Boot# usb reset
(Re)start USB...
USB: scanning bus for devices... No USB Device found
scanning bus for storage devices... 0 Storage Device(s) found
U-Boot# usb info
Configuration: 0
- Interfaces: 0 Bus Powered 0mA

Of course I had a USB stick in USB1 while testing this :-).

Any suggestions to make USB work?

Thanks and best reagrds,

Daniel