Hi.
we are using NTSC signal, 16ch CIF 30fps recording setting, progressive mode, RDK03.00.00.00
when i play video stream. sometimes free buffer (thrObj->bufQFreeBufs) is empty and playback video data stop and go .
i'm not using OSA_que because OSA_que use timeout (OSA_TIMEOUT_FOREVER).
we are tested subtitle passed tv news video data, at the times freebuffer empty, playback video stop and go . when i look closely.
i think , it's not a bandwidth issue because all 16 channel is a CIF video data.
is there any point of improvement such as check return value of function or print the value or increase of buffer size?
i suspect why freebuffer empty , sometimes freebuffer empty is lasted over milliseconds(100 milli over).
Best Regards.
CHO.