Other Parts Discussed in Thread: AM3358, TLK110
Hi,
We are debugging AM3358 EtherCAT board.
Problem: IN port seems to be working but OUT port is not working.
I already read this forum aout OUT port issue, and applied recent firmware 1.0.0.6.
But the result is same.
Our design is little different from ICE board.
Some pins are remaped, about TLK110's we changed only the reset pin of the OUT port.
And we use DDR3 DRAM not like DDR2 of ICE board.
I know only the PRU control the phy chips wholly, and CPU does not concerned.
Is it correct?
Is the PRU can control the reset pin also, and can be used with DDR3?
Is there any timing issue on PRU if we use DDR3?
So some EtherCAT function could be spoiled?
I guess it may not be a problem because IN port works well.
But I need your confirmation.
And I read PG1.0 has silicon bug concerned about OUT port function.
What means PG?
We have the chip marking
AM3358ZCZD72
2AACY2W GI
962 ZCZ
Is PG2.0 and has no probem about OUT port?
Thanks.
Regards.