hi,
i have a problem about DM8148 system mmu, if i enable the mmu, when call a forbid memory address, can it trigger a interrupt on the c674 DSP side?
and can the MMU_FAULT_PC return instruction address where call the forbid memory address?
and i has know the MMU_FAULT_AD can return the forbid address value.
also the mmu can set as user mode read/write/execute or Privileged Mode read/write/execute?
thanks!