Can you please advise on the best way to minimise power consumption when the following pins or functions are not used in a C5505A based system?
1) I2C Bus: SDA(B8) and SCL(B9) do not have internal pull-up or pull-down resistors. Should external pull-ups be fitted if the I2C bus is not used?
2) Wakeup (E8): Does this need to be terminated or should it be set as an output and driven low?
3) The EMIF bus: All Pins but D[0..15] and A[15..20] have a specific note to externally terminate the pin if unused.
3a) What is the best way to make this interface safe?
3b) Can any termination be achieved without discrete components?
3c) Can the EMIF D[0..15] pins be left floating or should these be terminated in some manner?
Sorry if this is already documented somewhere, but I couldn't find a suitable reference.
Thanks,
John