This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 USB peripheral mode

Hi,

We use the DM365 with linux 2.6.18 (Monta Vista).  The USB driver works in  pheripheral mode:

                        musb_hdrc: version 6.0, cppi-dma, peripheral, debug=0
                        musb_hdrc musb_hdrc: No DMA interrupt line
                        musb_hdrc: USB Peripheral mode controller at c3868000 using DMA, IRQ 12
                        g_file_storage gadget: File-backed Storage Gadget, version: 28 November 2005
                        g_file_storage gadget: Number of LUNs=1
                        g_file_storage gadget-lun0: ro=0, file: /dev/mmcblk0p1

When we connect USB cable between the bord  and a host PC, we have:

                       g_file_storage gadget: high speed config #1

Everything works and we can get files  from the SD card. But, transfer rate is not high.

To copy a file to the PC, the transfer rate is 4MB/s with a VFAT SD card  (SandDisk 16G class 4).  We tried other SD cards, but the speed is not changing.

Is it possible to have higher transfer speeds (~ 10MB/s)? How can we improve this transfer rate?

If you have ideas, we need help.

Thank you in advance.

SAKHO