Hello,
I know it could be dummie questions, but I still have to do it.
I am designing a pcb with the omap-l138 processor and a ddr2 memory. First at all I understand that the routing is in the first layer, only, ¿Is that right?
Secondly, there is a zone called keep out region and let's suppose that this region has an area: (A.P.), and is smaller that the layout area, I guess that the ground area below the first layer should match with the A.P. position, but, CanI use the rest area in the first and second(ground) and power layer (the third layer) outside the keep out region?
I guess the answer to both questions is: yes, but I have to be sure, if there is something that I should keep in mind, please tell me.
Thank you for your attention
Daniel