Hi,
we are using The Alaska® Ultra 88E1111 Gigabit Ethernet Trans-ceiver for interfacing with c6678.with SGMII.
Schematic reference for 1Giga bit is available
http://www.advantech.com/Support/TI-EVM/6678le_download.aspx from pages 27-29
In order to save power consumption we have changed our schematic with 100Mbit.
we have added pulse transfomer 10/100 BASE magnetics(in place of RJ45) takes inputs
from MDI0+, MDI0- to TD+, TD- MDI1+, MDI1- to RD+,RD- .
MDI2+, MDI2-, MDI3+ & MDI3- are connected to ground with 0 ohms resistor. Rest of schematic remains unchanged.
When we connected ethernet port to laptop it is showing 10Mbps. while debugging with c6678 emulator SGMII linkup flag is not setting. Also led linkup is not coming.
Pulse transfomer magnetics TX+ TX- are connected to PC RX+ , RX- and RX+, RX- are connected to PC TX+, TX- .
connections wise no issues. We have used same pulse transformer in blackfin inbuilt phy (its MII interface)controller it is working.
I guess SGMII tx configuration needs to be done if any one knows what exactly needs to be done please help.
Please let me know how to solve this issue.
regards
SrinivasPrasad