This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

openCV on DM6467

Hi guys,

I want use opencv on DM6467 could you give me some suggestion?

The first thing is port openCV to dsp? 

Then use C6Accel to call dsp openCV code?

I'm a new comer for DM6467, is this right or there is some other solution?

I followed the page  http://processors.wiki.ti.com/index.php/Using_C6Accel_on_DM6467_with_DVSDK_3.x

for this step: "Extract the codec package to subdirectory /cs2dm6467_1_00_00_10 and the C6Accel package to subdirectory c6accel_1_01_00_00."

but I can't find where to download the codec package and C6Accel package.

can anyone tell me where to download these two packages?

thanks a lot.