Other Parts Discussed in Thread: SYSBIOS, AM3358, AM3359, TLK110
Hello,
i tried the enetLwip sample from am335x_sysbios_ind_sdk_1.0.0.6, but it´s not working. It´s the same problem with CCS5 and the SD-Card.
The problem is:
Port 1 IP Address Acquisition Failed.
*** StarterWare Boot Loader. Build - ***
Copying application image from MMCSD to RAM
Copying to RAM completed successfully
Image Copy Successful, Executing Application..
TI Industrial SDK Version - 1.0.0.6
Device name : AM3358
Chip Revision : AM335x ES1.0 [PG1]
ARM Clock rate : 600
SYS/BIOS enetLwip Sample application running on ICE
Acquiring IP Address for Port 1
Port 1 IP Address Acquisition Failed.
Can somebody help me?
best regards
Stefan