This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MIPI DSI Driver: "omapdss DSI error: failed to set complexio power state to 1"

Other Parts Discussed in Thread: SYSCONFIG

Hi, we have to use pandaboard (OMAP4460) for driving LCD with MIPI DSI Interface (Video mode). Using Linaro's kernel.

We got the error message when boooting on  --> "omapdss DSI error: failed to set complexio power state to 1"

We do not know how to fit it. Is it caused by the wrong setting of DSI_COMPLEXIO_CFG1? Thanks for your suggestion!

The parameter were listed below:

LCD's resolution: 540 * 960,

Pixel Clock: 154MHz

Our setting as:

struct omap_dss_device omap4_panda_lcd_device = { 

  .name   = "lcd",          

 .driver_name  = "panel-dsi",   

 .type   = OMAP_DISPLAY_TYPE_DSI,   

  .data   = &panel_dsi_data, 

  .phy.dsi  = { 

  .clk_lane       = 3,   

.clk_pol        = 0,  

 .data1_lane     = 1,  

 .data1_pol      = 0,   

.data2_lane     = 2,   

 .data2_pol      = 0,

.type  = OMAP_DSS_DSI_TYPE_VIDEO_MODE,   

   }, 

 .clocks = {    

          .dispc = {      

                      .channel = {       .lck_div = 1, // LCD                                 

                                               .pck_div = 5, // PCD       

                                                .lcd_clk_src = OMAP_DSS_CLK_SRC_DSI_PLL_HSDIV_DISPC,   

                            }, 

                  .dispc_fclk_src = OMAP_DSS_CLK_SRC_DSI_PLL_HSDIV_DISPC,    

     }, 

   .dsi = {     

              .regn  = 16, // DSI_PLL_REGN      

               .regm  = 180, // DSI_PLL_REGM     

                .regm_dispc = 5, // PLL_CLK1 (M4)     

                  .regm_dsi = 5, // PLL_CLK2 (M5)     

                .lp_clk_div = 10, // LPDIV 

    .dsi_fclk_src   = OMAP_DSS_CLK_SRC_DSI_PLL_HSDIV_DSI,    

   }, 

  },   

  .channel  = OMAP_DSS_CHANNEL_LCD,   };

static struct omap_video_timings panel_dsi_timings = {

  .x_res = 540,  

  .y_res = 960,

   .pixel_clock = 154000, //80842,

    .hfp = 62,  

    .hsw = 4,  

     .hbp = 154,

       .vfp = 84,  

     .vsw = 1,  

     .vbp = 15,

 };

static const struct omap_dss_dsi_videomode_data vm_data = {        

 .hsa = 1,  

 .hfp = 115,   

.hbp = 47,    

 .vsa = 1,       

  .vfp = 84,        

 .vbp = 15,

 .vp_de_pol = true,        

 .vp_vsync_pol = true,       

  .vp_hsync_pol = false,        

 .vp_hsync_end = false,        

 .vp_vsync_end = false,

 .window_sync = 4,

};

THANKS

root@android:/ # cat /d/omapdss/dsi1_regs

DSI_REVISION                        00000030

DSI_SYSCONFIG                       00000015

DSI_SYSSTATUS                       00000001

DSI_IRQSTATUS                       00000180

DSI_IRQENABLE                       0015c000

DSI_CTRL                            00000100

DSI_COMPLEXIO_CFG1                  48000213

DSI_COMPLEXIO_IRQ_STATUS            00000000

DSI_COMPLEXIO_IRQ_ENABLE            3ff07fff

DSI_CLK_CTRL                        00044001

DSI_TIMING1                         7fff7fff

DSI_TIMING2                         7fff7fff

DSI_VM_TIMING1                      00000000

DSI_VM_TIMING2                      00000000

DSI_VM_TIMING3                      00000000

DSI_CLK_TIMING                      00000101

DSI_TX_FIFO_VC_SIZE                 00000000

DSI_RX_FIFO_VC_SIZE                 00000000

DSI_COMPLEXIO_CFG2                  00000000

DSI_RX_FIFO_VC_FULLNESS             00000000

DSI_VM_TIMING4                      00000000

DSI_TX_FIFO_VC_EMPTINESS            00000000

DSI_VM_TIMING5                      00000000

DSI_VM_TIMING6                      00000000

DSI_VM_TIMING7                      00000000

DSI_STOPCLK_TIMING                  00000080

DSI_VC_CTRL(0)                      00000000

DSI_VC_TE(0)                        00000000

DSI_VC_LONG_PACKET_HEADER(0)        00000000

DSI_VC_LONG_PACKET_PAYLOAD(0)       00000000

DSI_VC_SHORT_PACKET_HEADER(0)       00000000

DSI_VC_IRQSTATUS(0)                 00000000

DSI_VC_IRQENABLE(0)                 000000db

DSI_VC_CTRL(1)                      00000000

DSI_VC_TE(1)                        00000000

DSI_VC_LONG_PACKET_HEADER(1)        00000000

DSI_VC_LONG_PACKET_PAYLOAD(1)       00000000

DSI_VC_SHORT_PACKET_HEADER(1)       00000000

DSI_VC_IRQSTATUS(1)                 00000000

DSI_VC_IRQENABLE(1)                 000000db

DSI_VC_CTRL(2)                      00000000

DSI_VC_TE(2)                        00000000

DSI_VC_LONG_PACKET_HEADER(2)        00000000

DSI_VC_LONG_PACKET_PAYLOAD(2)       00000000

DSI_VC_SHORT_PACKET_HEADER(2)       00000000

DSI_VC_IRQSTATUS(2)                 00000000

DSI_VC_IRQENABLE(2)                 000000db

DSI_VC_CTRL(3)                      00000000

DSI_VC_TE(3)                        00000000

DSI_VC_LONG_PACKET_HEADER(3)        00000000

DSI_VC_LONG_PACKET_PAYLOAD(3)       00000000

DSI_VC_SHORT_PACKET_HEADER(3)       00000000

DSI_VC_IRQSTATUS(3)                 00000000

DSI_VC_IRQENABLE(3)                 000000db

DSI_DSIPHY_CFG0                     1e481d3a

DSI_DSIPHY_CFG1                     420a1a6a

DSI_DSIPHY_CFG2                     b800001a

DSI_DSIPHY_CFG5                     60000000

DSI_PLL_CONTROL                     00000000

DSI_PLL_STATUS                      000001c9

DSI_PLL_GO                          00000000

DSI_PLL_CONFIGURATION1              1081681f

DSI_PLL_CONFIGURATION2              00656008

 

root@android:/ # cat /d/omapdss/dispc_irq

period 572101 ms

irqs 0

FRAMEDONE                     0

VSYNC                         0

EVSYNC_EVEN                   0

EVSYNC_ODD                    0

ACBIAS_COUNT_STAT             0

PROG_LINE_NUM                 0

GFX_FIFO_UNDERFLOW            0

GFX_END_WIN                   0

PAL_GAMMA_MASK                0

OCP_ERR                       0

VID1_FIFO_UNDERFLOW           0

VID1_END_WIN                  0

VID2_FIFO_UNDERFLOW           0

VID2_END_WIN                  0

VID3_FIFO_UNDERFLOW           0

VID3_END_WIN                  0

SYNC_LOST                     0

SYNC_LOST_DIGIT               0

WAKEUP                        0

FRAMEDONE2                    0

VSYNC2                        0

ACBIAS_COUNT_STAT2            0

SYNC_LOST2                    0

 THANKS.... Best Regard, Owen