This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

setting resolution via xrandr

it running ubuntu with Xfce on TI 8148 evm board.

Where do I add the xrandr command to run it always after boot/startup automatically?    
i've put "xrandr -s 800x600 -r 60" command in /etc/init.d/rc.local , but getting "Can't open display "